..do most plants experience costly unplanned downtimes?

..do most plants over-lubricate or under-lubricate?

..is effective lubrication critical for worker safety?

..is your lubrication checklist as important as your production plan?

..invest in lubrication systems with longer service life?

..does the total cost of ownership matter more than unit price?

..is effective lubrication lowering emmisions?

..does energy efficiency start with lubrication?

..is training your team on lubrication essential?

..should lubrication be a skill - not just a task?

..do most plants experience costly unplanned downtimes?

..do most plants over-lubricate or under-lubricate?

..is effective lubrication critical for worker safety?

..is your lubrication checklist as important as your production plan?

..invest in lubrication systems with longer service life?

..does the total cost of ownership matter more than unit price?

..is effective lubrication lowering emmisions?

..does energy efficiency start with lubrication?

..is training your team on lubrication essential?

..should lubrication be a skill - not just a task?


Select

Purchase

Storage

Transfer

Application

Monitoring

Reconditioning / Disposal

Planning
Procedures
Training

Due to poor lubrication practices, 36% of bearing failures result from inadequate lubrication, and this number increases to 56% when contamination is also considered, making it the single largest cause of machine failure. Research shows that improper lubrication increases friction, wear, and overheating, directly leading to unexpected breakdowns and costly downtime.

Lubrication is often treated as a routine task rather than a precision process. Research shows that over 60% of lubrication-related failures are caused by incorrect quantity or frequency, either too much, leading to seal damage and overheating, or too little, resulting in friction and wear.

Poor lubrication can cause equipment to overheat, seize, or leak, creating slip hazards and increasing the risk of mechanical accidents. SKF highlights that lubrication failures can lead to catastrophic equipment breakdowns, endangering nearby personnel. One of the key benefits of automatic lubrication systems is that they reduce the need for manual access to moving or hazardous areas.

Without a structured lubrication checklist, even the most efficient production plan is vulnerable to unexpected breakdowns, safety risks, and costly delays. According to SKF’s lubrication maturity models, plants that implement detailed lubrication checklists experience significantly fewer failures and reduced maintenance costs. These checklists cover critical areas such as lubricant selection, storage and handling, application methods, contamination control, and condition monitoring, all of which directly impact uptime, safety, and operational efficiency.

It has been observed that automated lubrication systems reduce manual labor and extend re-lubrication intervals, saving up to $57,000 annually per machine in labor costs alone. They also significantly extend machine life, reduce human error, and improve consistency.

Focusing only on lubricant price overlooks hidden costs such as downtime, labor, and energy inefficiency. SKF’s lifecycle cost models show that premium lubrication systems pay for themselves through reduced failures and energy savings.

SKF’s sustainability data shows that optimized lubrication reduces CO₂ emissions and lubricant waste, supporting ESG goals. Automatic lubrication saves around 200,000 tons of grease per year worldwide by minimizing the waste caused by manual lubrication, equivalent to a reduction of 300,000 tons of CO₂. Additionally, SKF's RecondOil technology enables a circular use of oil that reduces CO₂ emissions by more than 96% overall.

A 2017 study cited by SKF found that 20% of global energy is lost to friction. Proper lubrication helps reduce this loss, improving machine efficiency and lowering energy bills.

SKF advocates a competency-based approach to lubrication, which involves understanding tribology, contamination control, and system design skills that directly impact plant performance and safety.

A leading research agency emphasizes that lubrication is a skill-based discipline, not just a routine task. Their training programs demonstrate that well-trained teams make better decisions, reduce errors, and extend equipment life.
Why is the right selection of lubricant important?
Choosing the correct lubricant prevents premature wear and breakdowns. SKF reports that 36% of bearing failures are attributed to poor lubrication, emphasizing the importance of matching lubricant properties to operating conditions for reliability.
It has a significant impact on:
Why is the right purchase strategy important?
A well-defined purchase strategy is essential for effective lubrication management because it ensures the selection of high-performance lubricants that align with equipment needs and operating conditions. Purchasing decisions should consider lifecycle cost, compatibility, and supplier support, not just unit price, to avoid failures and inefficiencies. This approach also supports sustainability goals by reducing lubricant waste and energy consumption.
Why is the right storage important?
Since the lubricants won’t be used immediately, proper storage is essential to prevent degradation even in sealed containers. Factors like temperature, humidity, and contamination from improper tools can compromise quality. SKF stresses the importance of climate-controlled storage, revised layouts, and color-coded, clean tools to avoid cross-contamination and maintain integrity. It also recommends first-in, first-out rotation, clear labeling, and filtration during transfer to sustain performance and extend shelf life.
Why are the right transfer techniques important?
Improper transfer introduces contaminants like dirt, water, and metal particles. Reports show that up to 56% of bearing failures are caused by contamination during handling and transfer. SKF emphasizes that using sealed, filtered, and color-coded transfer containers preserves lubricant quality and prevents cross-contamination, which directly impacts equipment reliability and safety.
Why selecting right method of application is important?
The 5Rs principle—Right lubricant, Right quantity, Right time, Right point, and Right method—is a foundational framework for selecting and applying lubrication systems effectively. According to SKF, this principle ensures that lubrication is not just performed, but optimized for reliability, safety, and efficiency across departments.
● The first three Rs (lubricant, quantity, time) are based on machine conditions and re-lubrication intervals.
● The fourth R (right point) involves tagging and color-coding to avoid cross-contamination.
● The fifth R (right method) helps decide between manual and automatic lubrication based on asset criticality and maintenance maturity
Why is right monitoring important for critical equipment?
Monitoring ensures that lubricants perform as intended—protecting components, minimizing wear, and preventing failures. SKF highlights that lubricant analysis and condition-based monitoring (e.g., vibration, thermography, ultrasound) help detect early signs of contamination or misapplication. SKF research shows 56% of bearing failures are due to poor lubrication and contamination, preventable through proactive monitoring.
Why the correct method for recondition and disposal helps save our environment?
Reconditioning used oil converts it from a waste product into a reusable resource, which can reduce environmental impact and operational costs. SKF reports that technologies such as RecondOil’s Double Separation Technology (DST) can regenerate oil to near-original condition, potentially lowering CO₂ emissions significantly, from 3,830 kg to 8.2 kg CO₂-eq per m³ of oil. A circular use of oil reduces CO2 emissions by more than 96%.